LaptopForums.Toshiba.com
Reply
Visitor
gk8325
Posts: 3
0

CD/DVD PLAYER Drive missing

L305-S5915 Can't use DVD Player. Error code19 Message reads cannot find specified drive.  MAT**bleep**ADVD-RAM UJ880AS (UF83 403918) Is there someplace I can download this?

Super Contributor
cee_64
Posts: 6,125
0

Re: CD/DVD PLAYER Drive missing

From Jerry_Lippey, one of our best Windows experts on the forums:

 

__________________________________________________

 

(Code 19)


That's the tip-off. You need a registry fix.

 

   Your CD drive or DVD drive is missing or is not recognized by Windows or other programs

-Jerry
-------------------------------------------------------------------------------------

If you don't post your COMPLETE model number it's very difficult to assist you. Please try to post in complete sentences with punctuation, capitals, and correct spelling. Toshiba does NOT provide any direct support in these forums. All support is User to User in their spare time.


Visitor
gk8325
Posts: 3
0

Re: CD/DVD PLAYER Drive missing

How do I do a registry fix?

Contributor
dan_g
Posts: 15
0

Re: CD/DVD PLAYER Drive missing

Click on the blue link left by Jerry,  Dan

Contributor
dan_g
Posts: 15
0

Re: CD/DVD PLAYER Drive missing

Hi, I found this, tried it and it worked. Only difference is I also had to uninstall device driver and restart after running it.

 

http://www.geekstogo.com/forum/CDgone-file8.html    ---- download the file, save it. run it. restart.; that should do it.

 

Dan

Super Contributor
Posts: 12,573
0

Re: CD/DVD PLAYER Drive missing

CDGone is supposed to do exactly the same thing as the one I gave you (KB314060).

 

It probably comes from Microsoft MVP Jim Eshelman's site.

 

Happy to learn you got the drive back in any case.

-Jerry
New Member
dennywj
Posts: 2
0

Re: CD/DVD PLAYER Drive missing

My DVD/CD-Rom is also missing.  It did work for over a year then it would be available sometimes and I would restart the laptop and it would be there.  Now it is completely gone.  Does not show up in the Device manager.  I tried the regedit but could not fine the Upper or lower filters where they were suppose to be.  Therfore I don't show any error codes.  The system cannot find it.  If I put a disk in and close it it appears to run up but nothing reads.

 

I don't have copies of the driver (Can't find it on the Toshiba web site) and am not sure where to look on the laptop and don't want to delete anything I not sure of and don't have a copy.  I cannot restore from the restore disks since it cannot read the CD's.

 

Help!!

 

New Member
nana55
Posts: 1
0

Re: CD/DVD PLAYER Drive missing

My complete model number is PSLD8U-0Q3033. Thank you for help. 

Super Contributor
Posts: 12,573
0

Re: CD/DVD PLAYER Drive missing

 

Satellite L355-S7905 

 


Thank you for help. 

What sort of help did you want, Nana?

-Jerry
Super Contributor
Posts: 12,573
0

Re: CD/DVD PLAYER Drive missing


Does not show up in the Device manager.


That ordinarily means the drive is dead.

-Jerry