LaptopForums.Toshiba.com
Reply
New Member
PooterDr
Posts: 1
0

XP drivers for A505-S6965

Please help! I need XP Pro x32 drivers for the Toshiba Satellite A505-S6965. Calls to Toshiba Tech Support were a waste of time - no help there, could not find the necessary XP drivers on the Support download page. Thanks in advance for your help. RK

New Member
lutalica
Posts: 2
0

Re: XP drivers for A505-S6965

Did you install XP (32) on your A505.

I would like to install XP on this great machine too.

I hate vista :-(

Any particular problem during installation?

How about drivers?

 

Thank you

Super Contributor
cee_64
Posts: 6,135
0

Re: XP drivers for A505-S6965


lutalica wrote:

Did you install XP (32) on your A505.

I would like to install XP on this great machine too.

I hate vista :-(

Any particular problem during installation?

How about drivers?

 

Thank you


Toshiba doesn't supply them.  You can try these drivers that someone uploaded for the A505-S5960.  Except for the Video Card they should be the same.  You'll probably need to get the Display Driver directly from ATI's support site.

 

 

--------------------8<------------------- <snip> ------------------

 

You need to make sure that your XP install disk is at least SP1 level or higher for it to recognize a hard driver larger than 137gb in size.  You can integrate SP1, 2, or 3 into your XP Instlal Disk by using nLite as per this guide.

 

Because Windows XP doesn't have native SATA support you'll need to do one of two things to install XP on your system.  You'll need to follow this guide to integrate your SATA drivers into your XP Install Disk.  DO yourself a huge favor and use the SATA drivers that they provide.  You can integrate your Service Packs during this proceedure as well.

 

The other option is as follows. 

 

--------------------8<------------------- <snip> ------------------

Switching back to AHCI (Runs a little faster than ATA mode)

 - First step is to install the basic Motherboard Chipset Driver and ONLY this driver. Do

not install anything else prior to installing the Intel Matrix Storage Manager Driver as

outlined below.

 

- Download the Intel Matrix Storage Manager here:
http://downloadcenter.intel.com/Product_Filter.aspx?ProductID=2101

- Once you download the file, run it with the -a switch:
    iata89_enu.exe -a


This will NOT install the Matrix Storage Manager. What this will do is run the installer, and

ONLY EXTRACT the files to C:\Program Files\Intel\Intel Matrix Storage Manager. Again, this

does NOT install anything.

 

- Your drivers are now located in C:\Program Files\Intel\Intel Matrix Storage Manager. They

will be found in either \Driver, or \Driver64, depending on whether you're running a 32-bit

or 64-bit OS.

- Go to Device Manager --> IDE ATA/ATAPI controllers. Double-click on the Intel ICH8M 3-port

SATA Controller - 2828... remember, *ONLY* click on the device that ends with 2828.

- Go to Driver tab, and choose to Update Driver.

- Tell the Wizard prompts:
- No, not this time
- Install from a list or specific location (Advanced)
- Don't Search. I will choose the driver to install.
- Click the "Have Disk" button. Point it to C:\Program Files\Intel\Intel Matrix Storage

Manager\Driver (or Driver64).
- Choose the driver you want to install....
- After you install the driver and click OK out of every menu, reboot the laptop.


-) During reboot, go into BIOS and turn on AHCI mode
--------------------8<------------------- <snip> ------------------

 

Install your drivers in this order.
Restart after each driver and take the time to test between drivers.
Some will apply and some won't.

 

Chipset software
Display driver
Sound driver
Modem Driver
If your machine has the internal WiFi card, then install the WLAN and/or WiFi driver
ACPI Common Modules (required for Power management tools to function)
Toshiba Console
Display Hotkey utility
Touchpad Driver
Touchpad enable/disable utility
Toshiba Network Device Switch utility
Toshiba Power Saver Utility
Toshiba Controls
Toshiba Utilities

--------------------8<------------------- <snip> ------------------

-------------------------------------------------------------------------------------

If you don't post your COMPLETE model number it's very difficult to assist you. Please try to post in complete sentences with punctuation, capitals, and correct spelling. Toshiba does NOT provide any direct support in these forums. All support is User to User in their spare time.