LaptopForums.Toshiba.com
Reply
Contributor
Helgen
Posts: 20
0

A205-S4777 CD/DVD Burning Fails EVERYTIME

I have Windows 7 installed, right, but it's not even W7's fault, Vista did the same thing. I downloaded the newest firmware, tried Alcohol 120%, DVD Decrypter, Windows on built in burners, nothing works.

 

I'm starting to this this laptop is the biggest piece of **bleep** ever made, since it doesn't even seem to want to load it's own SATA drivers when trying to install WXP (and doesn't have the option to change the SATA mode regardless firmware update or not.)

 

If someone can help me, please do, if not, I'm selling this.

Contributor
Helgen
Posts: 20
0

Re: A205-S4777 CD/DVD Burning Fails EVERYTIME

BUMP.