LaptopForums.Toshiba.com
Reply
Visitor
BlooJae23
Posts: 9
0

need help with several problems

i have a satellite L300 in february. it was working great until about 2 months ago. I'll start the computer, put my password in, wait for it to finish it's thing and then it freezes. and when it's not frozen it wont let me go on the internet. It says unidentifed network/limited access. it's connected to the router but wont connect to the internet pretty much. NEED HELP!!!!!

 

thank you much.....

 

 

 

BlooJae23  \m/(^_^)\m/

Super Contributor
Posts: 12,573
0

Re: need help with several problems

Try running the System File Checker.

 

   How to use the System File Checker tool to troubleshoot missing or corrupted system files on Windows...

 

Which Satellite L300?

-Jerry
Visitor
BlooJae23
Posts: 9
0

Re: need help with several problems

all the laptop says is satellite L300 System Unit.

Super Contributor
cee_64
Posts: 6,125
0

Re: need help with several problems

What is the PART Number?  It should look something like this:  PSLB0U-07K02D

-------------------------------------------------------------------------------------

If you don't post your COMPLETE model number it's very difficult to assist you. Please try to post in complete sentences with punctuation, capitals, and correct spelling. Toshiba does NOT provide any direct support in these forums. All support is User to User in their spare time.


Super Contributor
Posts: 12,573
0

Re: need help with several problems

There should be a label on the bottom with the part number.

-Jerry
Visitor
BlooJae23
Posts: 9
0

Re: need help with several problems

it's PSLB8U-08E04H

Super Contributor
Posts: 12,573
0

Re: need help with several problems

 


PSLB8U-08E04H

Satellite L300-ST2501 (PSLB8U-18D04H)

 

It's a variation of the one above. Probably made for some big-box retailer. All of the Toshiba drivers and utilities here should work.

 

Do you have Windows Vista on that computer? Which version?

 

Did you run the System File Checker I recommended?

-Jerry
Visitor
BlooJae23
Posts: 9
0

Re: need help with several problems

i tried to do the system check but my laptop keeps freezing before it can finish.

 

i have basic windows vista.

Super Contributor
Posts: 12,573
0

Re: need help with several problems


i have basic windows vista.


Give me the exact name and service-pack level.

 

Get those by running About Windows (winver.exe).

 

Mine, for example, says this.

 

   Windows Vista Ultimate

 

   Version 6.0 (Build 6002: Service Pack 2)

-Jerry
Visitor
BlooJae23
Posts: 9
0

Re: need help with several problems

Microsoft Windows

 

Version 6.0 (Build 6001: Service Pack 1)