LaptopForums.Toshiba.com
Reply
New Member
hrollur
Posts: 2
0

Re: Alps v7.102.302.101, Scroll/Browser stops working; have to restart to gain functionality

Actually I tried one driver I found on the US support site, I don't even know the models it was for but it seems to work perfectly for me.  It has a somewhat different software then the other ones, for example now when I scroll I get a Icon on screen that indicates scrolling.  But the good part is that I haven't had any problems since I installed it 2 days ago.  The driver is version 7.105.303.117 with alps software version 7.105.303.117 downloaded from here driver_touchpad_alps_TC70018700D.exe (toshiba website)

Super Contributor
Posts: 12,684
0

Re: Alps v7.102.302.101, Scroll/Browser stops working; have to restart to gain functionality

That's this one.

 

   ALPS Pointing Device Driver for Windows 7 (32/64) (Version 7.x5.303.117 - Released 10/21/09)

 


Applicable Models:
Satellite T115-S1100, T115-S1105, T115-S1108, T115-S1110, T135-SP2909R, T135-SP2909A, T135-SP2909C, T135-S1300RD, T135-S1305, T135-SP2911R, T135-S1312, T135-S1310WH, T135-S1310RD, T135-S1310, T135-S1309, T135-S1307, T135-S1305WH, T135-S1305RD, T135-S1300WH, T135-S1300, T135-SP2910A, T135-SP2910C, T135-SP2910R, T135-SP2911A, T135-SP2911C 
-Jerry
New Member
Hunter844
Posts: 1
0

Re: Alps v7.102.302.101, Scroll/Browser stops working; have to restart to gain functionality

I'm having the same problem and have yet to find a solution. I suspect the pad gets too hot and starts to flake out even after brief usage but who knows...it's a flaky pad no doubt.

 

 

Windows Vista 64 bit SP2

 

A3556935

 

 

Super Contributor
Posts: 12,684
0

Re: Alps v7.102.302.101, Scroll/Browser stops working; have to restart to gain functionality