LaptopForums.Toshiba.com
Reply
Super Contributor
Defender
Posts: 3,149

Re: How to Change Media Button Defult Program ?

Here is some assistance for that Europe model, post query there:   http://forums.computers.toshiba-europe.com/forums/thread.jspa?messageID=166503&#166503 some info there, PLUS sign into their Forum and post query.

 

As an interim measure try- open Control Panel/Hardware and Sound/Auto Play and reset as you desire.

New Member
tester07
Posts: 1
0

Re: How to Change Media Button Default Program ?

[ Edited ]

I ve got the same problem. And solved myself like that:

 

Go to registry:

HKEY_LOCAL_MACHINE\SOFTWARE\Toshiba\TBS\DefaultSetting\CDDVD\NOMEDIA

 

It should be like:

OPT1 = wmplayer.exe

OPT2 = /Task Media Library

 

And you need:

OPT1 = jetaudio.exe

OPT2 = "you can delete this values content, or you can write a jetaudio startup parameter like above"

 

Hope it works with your system.

Have a nice JET=)

 

&hope not too late:smileysad:

New Member
Mrowr623
Posts: 1
0

Re: How to Change Media Button Defult Program ?

Hello,

 

I changed the button to iTunes really easy.

The way i did it was that i went to:
Start

All programs

Toshiba

Utilities

Clicked Toshiba Assist

Clicked optimize

Clicked Toshiba Button Support

Changed "Button Name" to "CD/DVD"

Typed in the program you want in description, which was iTunes for me

Then for "Target Path" you click browse and select that program (you have to find the actual file location for the program) and then click register

Now, Everytime i click that button iTunes opens for me instead of that Media Player thing

 

Hope this helped, and if you were already helped, well that's good then. :smileyhappy:

New Member
Corby
Posts: 2
0

Re: How to Change Media Button Defult Program ?

I was able to use these instructions to change the button settings on my A215 so that it would open Windows Mail instead of Windows Media Player. Thank you very much.

Visitor
donman92
Posts: 2
0

Re: How to Change Media Button Default Program ?

I changed the registry values in order to open iTunes when I press the media buttons on my Toshiba A300 and it has worked O K.

 

..In a way of it loading iTunes like normal when pressed and having the ability to change track, play/pause, etc.

but when I minimize iTunes, I can't do any of those operations.

 

 

What do I have to change in order for iTunes to Fully integrate with the media buttons.

 

This is what I typed in for the registry changes:

 

 

OPT1 = itunes.exe

OPT2 = /Task Media Library

 

 

Visitor
donman92
Posts: 2
0

Re: How to Change Media Button Default Program ?

.. also

 

ima just stick to wmPlayer for now : /.

New Member
Corby
Posts: 2
0

Re: How to Change Media Button Default Program ?

I have the same problem, but it is not a flaw with the button program. It is a flaw with iTunes. I have the exact same problem on my desktop computer which I built myself, and I use a Microsoft Natural Multimedia Keyboard. Any other music player except iTunes uses the media buttons. Never have found a way around it.