LaptopForums.Toshiba.com
Reply
New Member
shackldfluffgrl
Posts: 4
0

Satellite P305D-S8829 touch pad buttons

The left mouse button below my laptop touch pad has stopped responding.  And so has the scroll option on the touch pad itself.  I tried to reinstall a driver but after it unzipped, nothing happened.  I restarted my laptop just to see if that'd get it to work and it didn't.  What should I do now?

Super Contributor
Posts: 12,667
0

Re: Satellite P305D-S8829 touch pad buttons

 

Satellite P305D-S8829 

 

Open Device Manager (devmgmt.msc), expand Mice and other pointing devices, and see if you have an Alps or Synaptics touchpad there. If so, which one?

 

Double-click it and tell us what Device status says.  

-Jerry
New Member
shackldfluffgrl
Posts: 4
0

Re: Satellite P305D-S8829 touch pad buttons

All it says is Alps Pointing Device

And under the status it says the device is working properly.

Super Contributor
Posts: 12,667
0

Re: Satellite P305D-S8829 touch pad buttons

Try reinstalling the driver.

 

   Alps Touch Pad Driver for Windows Vista

-Jerry
New Member
shackldfluffgrl
Posts: 4
0

Re: Satellite P305D-S8829 touch pad buttons

It didn't work.  The driver installed and I restarted but no luck.

Super Contributor
Posts: 12,667
0

Re: Satellite P305D-S8829 touch pad buttons

The only thing I can think of now is to open Mouse in Control Panel and fool around with likely-looking settings.

 

 

-Jerry
New Member
shackldfluffgrl
Posts: 4
0

Re: Satellite P305D-S8829 touch pad buttons

And if it doesn't work I just have to settle? 

Super Contributor
Posts: 12,667
0

Re: Satellite P305D-S8829 touch pad buttons

Other options are to plug in a real mouse (which I always use anyway) or restore the hard drive to its original factory-new state, which works when it's not a hardware malfunction.

-Jerry
Visitor
Egoetrexmeus
Posts: 2
0

Re: Satellite P305D-S8829 touch pad buttons

Exactly the same problem on my A505-S6960 ( no left click, no scrolling).. I tried system restore, it did not help..I suspect it's a hardware issue..Well, I still have a warranty.