LaptopForums.Toshiba.com
Reply
New Member
NAJ28
Posts: 1
0

Internal Database Error

Re:  Toshiba Satellite A105-S4002 (Model # - PSAA8U-05H00K)

 

Received the following message error when trying to access the internet via wireless connection (while logged on as the administrator) - internal database error when trying to update or save profile. 

 

No problems accessing wireless via Guest profile.  Any suggestions or fixes?

 

Super Contributor
Posts: 12,680
0

Re: Internal Database Error

 

Satellite A105-S4002 

 


internal database error when trying to update or save profile

No doubt you meant this message.


An internal database error occurred when saving/updating the profile

It probably comes from the Intel PROSet client. Won't hurt to reinstall both the driver and the client.

 

   Intel(R) 802.11a/b/g,b/g Driver V10.5.1.59/V9.0.4.17 & PROSet V10.5.0.1

-Jerry