LaptopForums.Toshiba.com
Reply
Contributor
scifi2nite
Posts: 12
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

So just an update, I went with Cyberdefender cause I really like the 24/7 computer support.  It has been very handy to have   I really like the interface - it's easy to use.  It has already pevented a couple of viruses and it's working good.  Just wanted to post an update.  I like it.

Contributor
PhlareHolmcross
Posts: 46
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

Norton Endpoint Protection for me. :smileyhappy:

 

Doesnt take that much resources from computer. Looks pretty good too.



Fixing Computers no Jutsu! (Ninja Help and Support Technique :smileyhappy:)
Contributor
trapweed
Posts: 11
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

I've used Cyberdefender for the last year now and absolutely swear by it!

Have lap, will top...
New Member
randommayham
Posts: 10
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

I wanted to jump in and give another praise for Cyberdefender.  Last week my daughter was having trouble with her printer not printing. I was on the road and directed her to call Cyberdefender.  They hleped her out right away - Cyberdefender rocks!

Contributor
Netname
Posts: 38
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

According to PC WORLD tests.

 

1. Norton Internet Security 2008

2. BitDefender IS (internet security) 2009

3. Panda IS 2009

4. McAfee IS 2009

5. Avira Premium IS 8.2

6. Kaspersy IS 2009.

7. F-Secure IS 2009.

8. Webroom IS Essentials

9. Trend Micro IS 2009

Super Contributor
Pensacola_Tiger
Posts: 891
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

Actually, the best anti-virus program is OS X Leopard.  Oh, yeah, you need to buy a Mac to use it though...

Contributor
trapweed
Posts: 11
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

I suggest CyberDefender because it cleans your PC of any existing problems then BLOCKS new virus' from attacking all while offering a 24/7 customer service!  I've not had any problems with it at all

Have lap, will top...
Regular Contributor
Joshuab2009
Posts: 70
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

I am using Norton Anti-Virus 2010, only because Toshiba gave it to me for a year and a half with my laptop. I used One Care at one time and was impressed with it. Also AVG has a full free version but its not live, just a scan.

________________
I am a student at DeVry University
New Member
passjam
Posts: 2
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

When all else fails Avast will find the last one and for home use it is free.

 

Started in computing in the Navy in 1965, it took a ship to carry one.

Regular Contributor
smitty1938
Posts: 75
0

Re: Which is the best anti-virus software program to use, if you want to buy it?

I have switched over to Microsoft Security Essentials. This is a free program and works extremely well. It can be found here.

 

http://www.microsoft.com/Security_Essentials/