LaptopForums.Toshiba.com
Reply
New Member
exene
Posts: 2
0

Archaic M205 Portege Assistance

Hi everyone.  I did a forum search and nothing really came up for the M205. 

My dilema is as follows...

 

I recently aquired this laptop (Portege M205) without an AC adapter.  I searched the toshiba website looking for any info on this model and I guess it's been discountied because nothing turned up in the search...

I don't have an AC adapter and the battery is fried so I cannot turn the thing on. ( I know it works it just needs the power adapter)

SO I guess my problem is this; Should I spend the $$$ on a power adapter to power it up and see what I can play around with in the system and add more memory, more disk space, etc. or should I just try to get rid of it.

 

I know it has the tablet edition windows and basically the stock specs, 512 RAM, 60GB hard drive, a pretty crappy video card, etc.

 

I just want to know if any of you guys think I would end up paying a crapload of money to get it turned on and fine tune this grandpa or since its so old just give it up??

 

Any advice would be awesome. Thanks.

Visitor
oldgazer
Posts: 9
0

Re: Archaic M205 Portege Assistance

If you really don't want it, I'll take it....

 

I have an M200, and it is sweet...  Its my first tablet PC.  I got it for nothing, but the HD had been wiped, so I had to get the restore DVD ($24.95 from Toshiba). I don't have a DVD drive, so I had do a PXE boot to restore across my network....

 

I would imagine eBay would be your best source for an adapter.  The one I have has the following part numbers...

 

M/N: PA3282U-1ACA

P/N: G71C0002S310

New Member
exene
Posts: 2
0

Re: Archaic M205 Portege Assistance

 

Hi thanks for the response.  I got an AC adapter from a neighbor for $45 dollars and powered up the portege.

Everything is running good except the battery doesn't hold the charge.

 

Okay so now I want to install factory settings on it.  How would I do this? Can I do it from F8 or F3 or F2? I dont have a disk or anything.. or is there somewhere I can download the file or something?

 

I used to have a dell 2 years ago and I was able to install factory from one of those keys... Ive never had a toshiba before so I dont know if it basically follows the same step..

 

thanks again

Super Contributor
cee_64
Posts: 6,154
0

Re: Archaic M205 Portege Assistance

You'll probably need to order replacement Recovery Media via this post though.  I don't think that system has an onboard recovery process.  Check out this document to see how Toshiba set's up the Recovery Process on their systems that have it.

-------------------------------------------------------------------------------------

If you don't post your COMPLETE model number it's very difficult to assist you. Please try to post in complete sentences with punctuation, capitals, and correct spelling. Toshiba does NOT provide any direct support in these forums. All support is User to User in their spare time.