LaptopForums.Toshiba.com
Reply
Visitor
MIDO
Posts: 6
0

DOES X305-Q710 HAVE A BLUETOOTH ???

Hi

 

I have  Qosmio X305-Q710

 

but I have a problem with the BLUETOOTH

 

this site tells it has 

 

http://www.toshibadirect.com/td/b2c/retail-product.jsp?poid=432323

 

but I can't find it

and when I try to install the driver

 

what would be the problem ??

It says "please plug in the Bluetooth device and ...."

what would be the problem ??

 

 

Thank you

 

 

Regular Contributor
Squall_Rinoa89
Posts: 163
0

Re: DOES X305-Q710 HAVE A BLUETOOTH ???

 


MIDO wrote:

Hi

 

I have  Qosmio X305-Q710

 

but I have a problem with the BLUETOOTH

 

this site tells it has 

 

http://www.toshibadirect.com/td/b2c/retail-product.jsp?poid=432323

 

but I can't find it

and when I try to install the driver

 

what would be the problem ??

It says "please plug in the Bluetooth device and ...."

what would be the problem ??

 

 

Thank you

 

 


yes the 701 has Bluetooth enabled. Only problem with it is the internet will be slower because both the Bluetooth AND Wireless uses the same signal so if your using wireless AND bluetooth it will cause some issues. Reason why is because your trying to connect a bluetooth device after your installing Bluetooth software/drivers.

 

 

Toshiba Qosmio X305-Q701 Owner
Sony PlayStation 3 60GB Owner
PSN: Squall_Rinoa89
I DON'T SUGAR COAT STUPIDITY
Super Contributor
Posts: 12,656

Re: DOES X305-Q710 HAVE A BLUETOOTH ???

 

Qosmio X305-Q710 

 

As the specs above show, you have the Bluetooth hardware installed.

 

Use Connect in Toshiba Assist to access the settings. See the section TOSHIBA Assist on p. 138 of the User's Guide.

 

   Qosmio X300 Series User's Guide

 

Windows Vista has its own Bluetooth support.

 

   Set up a Bluetooth enabled device

-Jerry
Visitor
MIDO
Posts: 6
0

Re: DOES X305-Q710 HAVE A BLUETOOTH ???

THANKS GUYS

 

I tried what you said

but I could solve it.

 

I don't find the Bluetooth sticker under my laptop  Is that a sign of the absence of the Bluetooth ???

 

If my laptop does not have an internal Bluetooth,Should TOSHIBA DO SOMETHING FOR ME ???

BECAUSE IT's Not My Fault .

 

 

THANK AGAIN

 

 

sorry for my English.

 

Super Contributor
Posts: 12,656
0

Re: DOES X305-Q710 HAVE A BLUETOOTH ???

Perhaps you need to reinstall the stack.

 

   Bluetooth Stack by Toshiba for Windows Vista / 7 (32bit/64bit)

-Jerry
Visitor
MIDO
Posts: 6
0

Re: DOES X305-Q710 HAVE A BLUETOOTH ???

I tried to reinstall the stack and this message

 "please plug in the Bluetooth device and ...."

 

comes again and again.

 

I believe my laptop isn't equipped with Bluetooth

 

and Unfortunately Toshiba lied to me .

Super Contributor
Posts: 12,656
0

Re: DOES X305-Q710 HAVE A BLUETOOTH ???


I believe my laptop isn't equipped with Bluetooth and Unfortunately Toshiba lied to me .


It's easy to find out whether the Bluetooth hardware is there. Perhaps it's malfunctioning.

 

Open Device Manager (devmgmt.msc) and expand Network adapters. Do you see a Bluetooth device there?

 

If so, double-click it and tell us what Device status is.

-Jerry
Visitor
MIDO
Posts: 6
0

Re: DOES X305-Q710 HAVE A BLUETOOTH ???

No, there isn't a Bluetooth device below Network adapters .

There are just the Intel wireless and Realtek LAN .

So what does that mean ?

 

Thank you again Jerry, I really appreciate your follow up .

Super Contributor
Posts: 12,656
0

Re: DOES X305-Q710 HAVE A BLUETOOTH ???


No, there isn't a Bluetooth device below Network adapters. So what does that mean ?


It means either the spec is wrong or the Bluetooth device is malfunctioning. I'll put my money on the latter.

 

If in warranty, time for service.

 

   Locate a Service Center

 

Or you can just add an adapter like this one.

 

   Toshiba Bluetooth USB Nano Adapter

-Jerry
Regular Contributor
Squall_Rinoa89
Posts: 163
0

Re: DOES X305-Q710 HAVE A BLUETOOTH ???

[ Edited ]

 


Jerry_Lippey wrote:

No, there isn't a Bluetooth device below Network adapters. So what does that mean ?


It means either the spec is wrong or the Bluetooth device is malfunctioning. I'll put my money on the latter.

 

If in warranty, time for service.

 

   Locate a Service Center

 

Or you can just add an adapter like this one.

 

   Toshiba Bluetooth USB Nano Adapter


 

Bluetooth Spec isnt there and u wont find it on the laptop anywheres and you wont find it in the system config irther.  You need to go down to "Toshiba" in the start menu and install it before it ever shows up Turn off search for Bluetooth divice when you first install it. Bluetooth Device on the laptop uses the SAME signal as your wireless unfortunately.

 

  • Built-in Devices Subwoofer , Four speakers , Bluetooth antenna , Wireless LAN antenna

 

http://reviews.cnet.com/laptops/toshiba-qosmio-x305-q710/4507-3121_7-33508115.html?tag=mncol;rnav

Toshiba Qosmio X305-Q701 Owner
Sony PlayStation 3 60GB Owner
PSN: Squall_Rinoa89
I DON'T SUGAR COAT STUPIDITY