LaptopForums.Toshiba.com
Reply
Visitor
deltanu22
Posts: 9
0

Toshiba Satellite A15-S157 website loading problems

[ Edited ]

Hello. First, thanks for reading my post and trying to help me out.

 

I have a Toshiba Satellite A15-S157.

Celeron CPU 2.2 2.19 GHZ

496 MB Ram

Windows 2002 Home Edition

Service Pack 2

Graphics Card: Intel Extreme 82852/82855 GM/GME Graphics Controller

Driver Version: 6.13.103514.

I'm running 1024x768 - 32 bit. I have OPEN GL.

 

I have all the latest updates from Windows and I believe I have all the updates for Toshiba drivers, bios etc, as well.

 

I have IE 7 with all the updates. Latest updates from Java, Shockwave. Adobe flash, etc.

 

I also downloaded Firefox version 3.0.9 for Windows to see if it was just the browser. Not the case.

 

Both security settings of the browsers are set to default.

 

My problem is the frames on the websites are not loading correctly. I don't know if because my computer is so old - it doesn't want to load these correctly but I've searched and searced for answers and I can't find an answer.

 

Now, I'm hoping you guys can help me out. I really really don't know why this is happening. All the flash ads are running but not the small stuff. Is it frameworks issues? I don't know if it's a graphics card issue. An "Manage add ons issue" or what. I thank you for any help. I attached a few photos for a visual reference.

 

Thanks

daron

deltanu22@yahoo.com

Screen Print 1

screen print 2

 

 

 

 

 

Super Contributor
Posts: 12,681
0

Re: Toshiba Satellite A15-S157 website loading problems

Satellite A15-S157 

My problem is the frames on the websites are not loading correctly.

 

All the flash ads are running but not the small stuff.


 

 Hard for me to see what doesn't look right.

 Take a look at your Hosts file. Paste it into your reply if it's not too big. You'll find it in this folder.

 

   %systemroot%\system32\drivers\etc

 

(Paste that path into Run from the Start menu.)

 

 

-Jerry
Visitor
deltanu22
Posts: 9
0

Re: Toshiba Satellite A15-S157 website loading problems

Hi Jerry,

Thanks for taking the time out to help me. It's really appreciated.

 

 

You mentioned "Hard for me to see what doesn't look right."

 

Here are two links to help see the differences:

What my computer is producing

http://farm4.static.flickr.com/3514/3465587669_d611e6dfbc_o.jpg 

What Yahoo should look like

http://farm4.static.flickr.com/3615/3473778880_125e6b6220_o.jpg

 

 " Take a look at your Hosts file."

 Here is my host file:

Copyright (c) 1993-1999 Microsoft Corp.
This is a sample HOSTS file used by Microsoft TCP/IP for Windows.
This file contains the mappings of IP addresses to host names. Each
 entry should be kept on an individual line. The IP address should
 be placed in the first column followed by the corresponding host name.
 The IP address and the host name should be separated by at least one
 space.

 Additionally, comments (such as these) may be inserted on individual
 lines or following the machine name denoted by a '#' symbol.

 For example:

      102.54.94.97     rhino.acme.com          # source server
       38.25.63.10     x.acme.com              # x client host
       127.0.0.1       localhost

 

Super Contributor
Posts: 12,681
0

Re: Toshiba Satellite A15-S157 website loading problems

 

That's an interesting puzzle, Daron!

 


Service Pack 2 .... I have all the latest updates from Windows


 

Any reason you've not updated Windows to SP3?

I realize that this occurs for both IE and Firefox, but humor me by resetting IE7.

 

   How to reset Internet Explorer settings

-Jerry
Visitor
deltanu22
Posts: 9
0

Re: Toshiba Satellite A15-S157 website loading problems

SP3 wasn't much of an upgrade so I didn't do it and I read some issues out there I didn't want to chance.  Resetting the manufactuer's setting for IE7 DID NOT work unfortunately.  I'm downloading IE8 now - to see if that makes a difference.  But I had this same problem with IE 6 hoping IE7 would change it.  I'm not sure if it's a graphics driver or what but it's really weird. Been trying to work this problem out for several years now.  If you have any other suggestions, they're greatly appreciated. Thanks, Jerry. Daron
Super Contributor
Posts: 12,681
0

Re: Toshiba Satellite A15-S157 website loading problems


I'm downloading IE8 now - to see if that makes a difference.

I have no reason to believe it will, Daron.

 


Been trying to work this problem out for several years now.

You must have reinstalled the display driver during that time. If not,....

 

   Windows XP/2000 Display Driver for Intel Montara GML display adapters

-Jerry
Visitor
deltanu22
Posts: 9
0

Re: Toshiba Satellite A15-S157 website loading problems

You are right IE8 didn't do anything. Should I reinstall the driver via the link above?
Visitor
deltanu22
Posts: 9
0

Re: Toshiba Satellite A15-S157 website loading problems

I went ahead and reinstalled the driver. I remember doing that before.

 

Still no change.

 

: (

 

Super Contributor
Posts: 12,681
0

Re: Toshiba Satellite A15-S157 website loading problems

Never seen this before. Maybe some kind of minor corruption in your WinSock settings. Try fixing those.

 

   Repair/Reset Winsock settings (Links)

-Jerry
Visitor
deltanu22
Posts: 9
0

Re: Toshiba Satellite A15-S157 website loading problems

Jerry,

Thanks so much for all your responses. Unfortunately the WINSOCK reset did not work. I ran the EXE through the link and crossed my fingers during the Restart. This is a tough one and I'm weirded out by why it's happening.

 

I looked around more this week and couldn't find anything. If you have any other suggestions, thanks.

Daron